[:SENSe]:CORRection:ENR:EXTRapolated?

(Read-Only) Queries the ENR table's extrapolation status (Extrapolation Enabled (1)/ Extrapolation Disabled (0).

Note: The ENR extrapolation status is only relevant when the CORRection:ENR:MODe is set to Table.

See also, [:SENSe]:CORRection:UCALibration:CANCel, [:SENSe]:CORRection:UCALibration:RUN, and [:SENSe]:CORRection:RCALibration:RUN, [:SENSe]:CORRection:RCALibration:CANCel, [:SENSe]:CORRection:UCALibration[:STATe], [:SENSe]:CORRection:USER:INTerpolated?, and [:SENSe]:CORRection:RCALibration[:STATe]?.

Relevant Modes

NF

Parameters

 

<not applicable>

 

Examples

n/a

Query Syntax

CORR:USER:EXTR?

Return Type

0 (False) - Extrapolation is disabled

1 (True) - Extrapolation is enabled

Default

not applicable


Last Modified:

01-june-2018

Added Opt. 356 NF(10.3)