|
(Read-Write) Set and query the kSSB of the signal SSB. See 5G NR physical channels and modulation (3GPP TS 38.211 version 15.7.0 Release 15) Section 4.4. |
|
|
Relevant Modes |
|
|
Couplings |
Only available when SSB Auto-Detect is disable. See [:SENSe]:NREVm:SSB:AUTO. This setting is coupled to the Resource Grid SCS setting. See [:SENSe]:NREVm:SCS |
|
Parameters |
|
|
<int/char> |
The kSSB value. The MINimum is 0. The MAXimum is dynamic and varies based on the Resource Grid SCS setting. This command will accept MINimum and MAXimum as arguments. |
|
Examples |
NREV:KSSB 4 */Sets the kSSB to 4 of the signal SSB |
|
Query Syntax |
NREV:KSSB? */queries the kSSB value of the signal SSB |
|
Return Type |
integer |
|
Default |
Varies based on Resource Grid SCS setting. |
Last Modified:
|
10jun2024 |
New command |