|
(Read-Write) Set and query the signal Lmax. See 5G NR physical layer procedures for control (3GPP TS 38.213 version 15.7.0 Release 15) Section 4.1. |
|
|
Relevant Modes |
|
|
Couplings |
Only available when SSB Auto-Detect is disable. See [:SENSe]:NREVm:SSB:AUTO. This setting is coupled to the Bandwidth setting. When an FR1 bandwidth is selected, 4 & 8 are available. When an FR2 bandwidth is selected, 64 is available. See [:SENSe]:NREVm:BANDwidth . |
|
Parameters |
|
|
<char> |
The Lmax value. Choose from: L4 - Lmax of 4 L8 - Lmax of 8 L64 - Lmax of 64 |
|
Examples |
NREV:LMAX L64 */Sets the signal Lmax to 64 |
|
Query Syntax |
NREV:LMAX? */queries the signal Lmax value |
|
Return Type |
character |
|
Default |
L4 |
Last Modified:
|
10jun2024 |
New command |