[:SENSe]:NREVm:RBOFfset <int>

(Read-Write) Set and query the Resource Block (RB) offset of the signal SSB relative to CRB0.

See 5G NR physical channels and modulation (3GPP TS 38.211 version 15.7.0 Release 15) Section 4.4.

Relevant Modes

5G EVM

Couplings

Only available when SSB Auto-Detect is disable. [:SENSe]:NREVm:SSB:AUTO.

This setting is coupled to the Resource Grid Start and Grid Size settings. See [:SENSe]:NREVm:GSTart and [:SENSe]:NREVm:GSIZe.

Parameters

 

<int>

The RB offset value.

The MINimum is dynamic and varies based on the Resource Grid Start setting.

The MAXimum is dynamic and varies based on the Resource Grid Start and Grid Size settings.

This command will accept DEFault, MINimum and MAXimum as arguments.

Examples

NREV:RBOF 166 */Sets the RB offset to 166

Query Syntax

NREV:RBOF? */queries the RB offset value

Return Type

integer

Default

Varies based on the Resource Grid Start and Grid Size settings.


Last Modified:

10jun2024

New command