|
(Read-Write) Set and query the resource grid size. See 5G NR physical channels and modulation (3GPP TS 38.211 version 15.7.0 Release 15) Section 4.4. |
|
|
Relevant Modes |
|
|
Couplings |
Only available when SSB Auto-Detect is disable. See [:SENSe]:NREVm:SSB:AUTO. This setting is coupled to the Bandwidth and SCS settings. See [:SENSe]:NREVm:BANDwidth and [:SENSe]:NREVm:SCS. |
|
Parameters |
|
|
<int/char> |
The resource grid size. The MINimum is 0. The MAXimum is dynamic and varies based on the Bandwidth and SCS settings. This command will accept MINimum and MAXimum as arguments. |
|
Examples |
NREV:GSIZ 273 */Sets the resource grid size to 273 |
|
Query Syntax |
NREV:GSIZ? */queries the resource grid size value |
|
Return Type |
integer |
|
Default |
Varies based on the Bandwidth and SCS settings. |
Last Modified:
|
10jun2024 |
New command |