|
(Read-Write) Set and query the signal subCarrierSpacingCommon. See 5G NR Radio Resource Control (RRC) Protocol Specification (3GPP TS 38.331 version 15.7.0 Release 15) Section 6.2.2. |
|
|
Relevant Modes |
|
|
Couplings |
Only available when SSB Auto-Detect is disable. See [:SENSe]:NREVm:SSB:AUTO. This setting is coupled to the Bandwidth setting. When an FR1 bandwidth is selected, 15 kHz & 30 kHz SCS are available. When an FR2 bandwidth is selected, 60 kHz & 120 kHz SCS are available. See [:SENSe]:NREVm:BANDwidth . |
|
Parameters |
|
|
<char> |
The subCarrierSpacingCommon value. Choose from: S15K - 15 kHz (µ=0) S30K - 30 kHz (µ=1) S60K - 60 kHz (µ=2) S120K - 120 kHz (µ=3) |
|
Examples |
NREV:SCS:COMM S30K */Sets the signal subCarrierSpacingCommon to 30 kHz (µ=1) |
|
Query Syntax |
NREV:SCS:COMM? */queries the signal subCarrierSpacingCommon value |
|
Return Type |
character |
|
Default |
Varies based on the Bandwidth setting. |
Last Modified:
|
10jun2024 |
New command |