|
(Read-Write) Set and query the signal SSB case. See 5G NR physical layer procedures for control (3GPP TS 38.213 version 15.7.0 Release 15) Section 4.1. |
|
|
Relevant Modes |
|
|
Couplings |
Only available when SSB Auto-Detect is disable. See [:SENSe]:NREVm:SSB:AUTO.
This setting is coupled to the Resource Grid SCS setting. The following SSB cases are available for the associated SCS: 15 kHz SCS - Case A 30 kHz SCS - Case B & C 120 kHz SCS - Case D 240 kHz SCS - Case E See [:SENSe]:NREVm:SCS. |
|
Parameters |
|
|
<char> |
The signal SSB case value. Choose from: A - Case A B - Case B C - Case C D - Case D E - Case E |
|
Examples |
NREV:SSB:CASE C */Sets the signal SSB to Case C |
|
Query Syntax |
NREV:SSB:CASE? */queries the signal SSB case |
|
Return Type |
character |
|
Default |
B |
Last Modified:
|
10jun2024 |
New command |