(Read-Write) Set and query the Blue power level limit used with Bar Chart displays (Option LTE FDD, 5G TF, 5G NR, and 5G NR EVM Conducted only). See also: [:SENSe]:POWer:RPLevel (Red power level) |
|
Relevant Modes |
|
Parameters |
|
<num> |
Select the LOWEST power levels (in dB) that you expect to measure. This power level, and those measured lower than this level, appear Blue. Enter a value between the 0 and the current Red (Highest) limit. (Default Red is -50) Couplings: If it’s over range with max value, Blue limit = Red limit -1 |
Examples |
POW:BPL -80 |
Query Syntax |
[:SENSe]:POWer:BPLevel? |
Return Type |
Numeric |
Default |
-90 |
Last Modified:
22-044-2026 |
Adding new command for LTE FDD & 5GTF (A.11.0) |