[:SENSe]:POWer:RPLevel <num>

(Read-Write) Set and query the Red power level limit used with Bar Chart displays (Option LTE FDD, 5G TF, 5G NR, and 5G NR EVM Conducted onlyfS).  

See also: [:SENSe]:SPECtrogram:BPLevel (Blue power level)

Relevant Modes

LTE FDD, 5G TF, 5G NR, 5G NR EVM Conducted

Parameters

 

<num>

Select the HIGHEST power levels (in dB) that you expect to measure. This power level, and those measured higher than this level, appear Red.

Enter a value between 0 and the current Blue (Lowest) limit. (Default Blue is -90).

Couplings: If it’s over range with min value, Red limit = blue limit + 1

Examples

POW:RPL -10

Query Syntax

[:SENSe]:POWer:RPLevel?

Return Type

Numeric

Default

-50


Last Modified:

03dec2018

Adding new command for LTE FDD & 5GTF (A.11.0)