|
(Read-Write) Set and query the channel number that appears in the center of the current channel measurement. First select a Radio Standard [:SENSe]:RADio:STANdard then activate the channel frequency-drive commands by changing [:SENSe]:RADio:TEUNit to CHAN. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<num> |
Channel number. The range of valid channel numbers depends on the current radio standard. If a channel number outside the acceptable range is entered, the channel will be set to the closest valid channel number. |
|
Examples |
RAD:CHAN:CENT 10 |
|
Query Syntax |
[:SENSe]:RADio:CHANnel:CENTer? |
|
Return Type |
Numeric |
|
Default |
Center channel of the radio standard. |
Last Modified:
|
1-Apr-2014 |
Added CPM |