[:SENSe]:SEMask:AVERage:COUNt <num>

(Read-Write) Set and query the SEM averaging count.

See also [:SENSe]:SEMask:AVERage:ENABle.

Relevant Modes

SA

Parameters

 

<numeric>

Choose from:

1 to 10000 number of satellites to display

This command accepts MIN and MAX to set the minimum power required.

Examples

SEM:AVER:COUN 27 'sets the SEM averaging at 27

SEM:AVER:COUN MAX 'sets the SEM averaging count to 10000

Query Syntax

SYSTem:GPS:AVERage:TOPN?

Return Type

numeric

Default

11


Last modified:

01nov2019

Added to SA