(Read-Write) Set and query the SEM averaging state. When ON averaging cycles through reference channel and all offsets n times. This produces a final averaged reference channel power. See also [:SENSe]:SEMask:AVERage:COUNt. |
|
Relevant Modes |
|
Parameters |
|
<booleon> |
Choose from: OFF (0) - Averaging is disabled. ON (1) - Averaging is enabled. |
Examples |
SEM:AVER:ENAB 0 'disables SEM averaging SEM:AVER:ENAB ON 'enables SEM averaging |
Query Syntax |
SEM:AVER:ENAB? |
Return Type |
numeric |
Default |
0 |
Last modified:
01dec2019 |
Added to SA |