(Read-Write) Set and query a fixed SEM power reference (which also fixes the Relative Limit Line). But then you must consider the unit being used (dBm or dBm/Hz) depending on the Measure Type selected. See also [:SENSe]:SEMask:MTYPe and [:SENSe]:SEMask:MREFerence:AUTO. |
|
Relevant Modes |
|
Parameters |
|
<numeric> |
Choose from: -1000 to 1000 (dBm or dBm/Hz) |
Examples |
SEM:MREF 100 'Sets the SEM power reference to 100 dBm or dBM/Hz. SEM:MREF MAX 'Sets the SEM power reference to 1000 dBm or dBM/Hz. |
Query Syntax |
SEM:MREF? |
Return Type |
numeric |
Default |
0.00E+00 dBm |
Last Modified:
01dec2019 |
New command |