(Read-Write) Set and query the power reference Auto state. When enabled the FieldFox tracks the measurement type and the automatically change the power reference units dBm or dBm/Hz. If the power reference is disabled, you must choose the correct units for the SEM measurement type. See also [:SENSe]:SEMask:MREFerence and [:SENSe]:SEMask:MTYPe. |
|
Relevant Modes |
|
Parameters |
|
<booleon> |
Choose from: OFF (0) - Averaging is disabled. ON (1) - Averaging is enabled. |
Examples |
SEM:MREF:AUTO 0 'disables the SEM power reference Auto setting. SEM:MREF:AUTO ON 'enables SEM power reference Auto setting. |
Query Syntax |
SEM:MREF:AUTO? |
Return Type |
numeric |
Default |
0 |
Last modified:
01dec2019 |
Added to SA |