(Read-Write) Set and query the sweep acquisition parameter. This effectively sets the sweep time in SA mode. Adjust this setting in order to increase the probability of intercepting and viewing pulsed RF signals. Also set [:SENSe]:SWEep:ACQuisition:AUTO to 0 (OFF). |
|
Relevant Modes |
EMI, SA, RTSA |
Parameters |
|
<num> |
Choose a relative acquisition value between 1 and 5000, where: 1 = Fastest sweep possible 5,000 = Slowest sweep possible. |
Examples |
SWE:ACQ 25 |
Query Syntax |
[:SENSe]:SWEep:ACQuisition? |
Return Type |
Numeric |
Default |
1 |
Last Modified:
10-june-2016 |
Added RTSA mode (9.50) |