[:SENSe]:SWEep:ACQuisition:AUTO <bool>

(Read-Write) Set and query sweep acquisition state.

Relevant Modes

EMI, SA, RTSA

Parameters

 

<bool>

Choose from:

ON or 1 - Automatically set to the fastest sweep possible with the current settings.

OFF or 0 - Manually set the acquisition parameter using [:SENSe]:SWEep:ACQuisition

Examples

SWE:ACQ:AUTO 1

Query Syntax

[:SENSe]:SWEep:ACQuisition:AUTO?

Return Type

Boolean

Default

ON or 1


Last Modified:

10-june-2016

Added RTSA mode (9.50)