[:SENSe]:SWEep:TIME <num>

(Read-Write) Set and query the sweep time of the measurement. The actual sweep time that is displayed on the screen will usually be higher than this value due to the overhead sweep time.

In SA mode, use this command for Zerospan measurements.

To set and read sweep time for Non-zerospan measurements in SA mode, use [:SENSe]:SWEep:ACQuisition.

Relevant Modes

CAT, EMI, NA, SA, RTSA

Parameters

 

<num>

Sweep time in seconds.

Examples

SWE:TIME .250

Query Syntax

[:SENSe]:SWEep:TIME?

Return Type

Numeric

Default

0


Last Modified:

10-june-2016

Added RTSA mode

17-Aug-2012

Added SA mode