(Read-Write) Set and query the periodic trigger synchronization source. The source used to synchronize/initialize the periodic trigger. To synchronize the periodic trigger, select the desired synchronization source, wait for the source event to occur (the instrument does not provide any indication when the source event occurs), then select None. NOTE: The instrument does not provide any indication when the source event occurs. |
|
Relevant Modes |
IQA, 5G NR, 5G NR EVM Conducted, 5GTF, SA, LTE FDD, PAA, RTSA |
Parameters |
|
<character> |
Periodic sync. Choose from: NONE - (None) Should be selected after synchronization with another source. Can also be used for an arbitrary periodic trigger. EXT - (External) - Synchronize to an external trigger signal. TPROX - Synchronize with the GPS 1 PPS signal. See Alson/a
|
Examples |
TRIG:PER:SYNC EXT */Sets the periodic trigger synchronize with an external trigger. TRIG:PER:SYNC TPROX */Sets the periodic trigger to synchronize with the GPS 1 PPS signal. |
Query Syntax |
TRIGger[:SEQuence]:SOURce? |
Return Type |
Character |
Default |
NONE |
Last Modified:
10dec2019 |
New command (11.5x) |