SYSTem:ANTenna:USB:AXIS <char>

(Read-Write) Set and query the USB triaxial antenna axis.

Relevant Modes

5G EVM, EMI, USB (EMF) Antenna, Pulse Generator

Couplings   

None

Parameters

 

<char>

<character> Component carrier (CC) value. Choose from:

AUTO – Manual axis control is disabled (off). All axes are selected and controlled by the instrument.

NOTE: Manual axis control was disabled by "N". This parameter is no longer valid.

X – X axis is selected for manual control.

Y – Y axis is selected for manual control.

Z – Z axis is selected for manual control.

Examples

SYST:ANT:USB:AXIS X */Selects the X axis for manual control.

Query Syntax

SYST:ANT:USB:AXIS?

Return Type

Character

Default

N (Manual axis control is off)


Last Modified:

04nov2022

Added EMI mode (12.3x)

01dec2019

New command