SYSTem:ANTenna:USB:TYPe <char>

(Read-Write) Set and query the USB triaxial antenna type.

Relevant Modes

5G EVM, EMI, USB (EMF) Antenna, Pulse Generator

Couplings

None

Parameters

 

<char>

Antenna-type choose from:

TRI – Sets the USB antenna-type to be triaxial.

Note: Only one USB triaxial antenna is compatible with the FieldFox.

Examples

SYST:ANT:USB:TYP TRI */Selects the USB antenna-type to triaxial.

Query Syntax

SYST:ANT:USB:TYP?

Return Type

Character

Default

TRI


Last Modified:

04nov2022

Added EMI mode (12.3x)

01dec2019

New command