(Read-Write) Set and query the status of the GPS averaging statistics displayed at the top of the C/No graph. Note: When enabled, this calculates the average power given the TOPN or MINP constraints. See also, SYST:GPS:AVER:MINP and SYST:GPS:AVER:TOPN. |
|
Relevant Modes |
All modes |
Parameters |
|
<char> |
Choose from: ON (1) - GPS Averaging statistics ON. OFF (0) - GPS Averaging statistics OFF |
Examples |
SYST:GPS:AVER 0 'Disables the displaying of the GPS averaging statistics |
Query Syntax |
SYSTem:GPS:AVER? |
Return Type |
Boolean |
Default |
OFF (0) |
Last modified:
01nov2019 |
Added for PAA Mode |
20-Jul-2010 |
New command (A.05.33) |