SYSTem:HEAD:POWer <num>

(Read-Write) Set and query the OML head frequency extender low power level. Once set, this low power level is used each time any OML head is connected to the FieldFox.

Relevant Modes

 5G NR, 5G NR EVM Conducted, 5G TF, IQA, LTE FDD, PAA, RTSA, SA

Parameters

 

<num>

Power level in dBm. Choose a value between -18 dBm and 0.

This command will accept MIN and MAX as arguments.

Examples

SYST:HEAD:POW -9 'Sets the LO power to -9 dBm.

SYST:HEAD:POW min 'Sets the LO power to minimum (-18 dBm).

Query Syntax

SYSTem:HEAD:POWer?

Return Type

Numeric

Default

-1.00E+01


Last Modified:

01nov2021

New command (A.12.35)