SYSTem:MAP:DISPlay:DEVice[:DESTination] <string>


(Read-Write) Set and query the type of device storage type for the destination location for storing indoor/outdoor maps (i.e., INT, USB, or SD).

See also, SYST:MAP:DISP:DEV:SOUR.

Relevant Modes

Channel Scanner, 5G NR, 5G TF, 5G NR EVM Conducted, LTE FDD, and PAA

Parameters

 

<"device">

Data capture device storage-type.

INT - internal FieldFox memory

SD - SD card

USB - USB storage device

Examples

SYST:MAP:DISP:DEV SD

Query Syntax

SYST:MAP:DISP:DEV?

Return Type

character

Default

INT


Last Modified:

09dec2019

Added new Mapping content (11.5x).