SYSTem:MAP:DISPlay:ICONs <string>


(Read-Write) Set and query the type of mapping icon being displayed.

Relevant Modes

Channel Scanner, 5G NR, 5G TF, 5G NR EVM Conducted, LTE FDD, and PAA

Parameters

 

<"icon">

Data mapping icon displayed.

FLAG - diplays a red flag icon (not available when LINE is set)

POInt - displays a point as the icon

LINE - displays a line connecting each point icon on the map

Examples

SYST:MAP:DISP:ICON FLAG */Sets the icon to a flag.

Query Syntax

SYST:MAP:DISP:ICON?

Return Type

character

Default

FLAG


Last Modified:

09dec2019

Added new Mapping content (11.5x).