SYSTem:MAP:DISPlay[:STATe]


(Read-Write) Enables or disables the map displayed on the FieldFox.

Relevant Modes

Channel Scanner, 5G NR, 5G TF, 5G NR EVM Conducted, LTE FDD, and PAA

Parameters

 

<booleon>

Enable/disable map labels.

0 - disable the map labels

1 - enable the map labels

Examples

SYST:MAP:DISP 1 */Sets the FieldFox to display the current map of latitude and longitude coordinates.

Query Syntax

SYST:MAP:DISP?

Return Type

INT

Default

0 (disabled)


Last Modified:

09dec2019

Added new Mapping content (11.5x).