:TRACe:IMAGinary:Y:DLINe <volt>

(Read-Write) Set and query the waveform imaginary line values.

See also TRAC:WAV:Y:DLIN, TRAC:REAL:Y:DLIN, TRAC:PHAS:Y:DLIN, and TRAC:UPH:Y:DLIN.

Note: Polar trace is not supported.

Relevant Modes

IQA

Parameters

 

<voltage>

Y-axis waveform imaginary level. Units depend on the selected setting. See :TRAC:WAV:AMPL:UNIT

Minimum: -9.9e37V

Maximum: 9.9e37V

Examples

TRAC:IMAG:Y:DLIN 1

Query Syntax

TRAC:IMAG:Y:DLINe?

Return Type

Numeric

Default

0V


Last Modified:

22oct2017

Added IQA mode (10.1x)