(Read-Write) Set and query the waveform unwrapped phase line values. See also TRAC:WAV:Y:DLIN, TRAC:REAL:Y:DLIN, TRAC:IMAG:Y:DLIN, and TRAC:PHAS:Y:DLIN. Note: Polar trace is not supported. |
|
Relevant Modes |
IQA |
Parameters |
|
<degree> |
Y-axis waveform unwrapped phase level. Units depend on the selected setting. See :TRAC:WAV:AMPL:UNIT Minimum: -360 degrees Maximum: 360 degrees |
Examples |
TRAC:UPH:Y:DLIN -180 |
Query Syntax |
TRAC:UPH:Y:DLINe? |
Return Type |
degrees |
Default |
0 degrees |
Last Modified:
22oct2017 |
Added IQA mode (10.1x) |