(Read-Write) Set and query the waveform real line values. See also TRAC:WAV:Y:DLINe, TRAC:IMAG:Y:DLIN, TRAC:PHAS:Y:DLIN, and TRAC:UPH:Y:DLIN. Note: Polar trace is not supported. |
|
Relevant Modes |
IQA |
Parameters |
|
<voltage> |
Y-axis waveform real level. Units depend on the selected setting. See :TRAC:WAV:AMPL:UNIT Minimum: -9.9e37V Maximum: 9.9e37V |
Examples |
TRAC:REAL:Y:DLIN 1 |
Query Syntax |
TRAC:REAL:Y:DLINe? |
Return Type |
Numeric |
Default |
0V |
Last Modified:
22oct2017 |
Added IQA mode (10.1x) |