(Read-Write) Set and query the type of SA Mode trace display state. Use [:SENSe]:QUANtity:TACTive? to read the number of active traces. |
|
Relevant Modes |
EMI, SA, RTSA |
Parameters |
|
<n> |
Trace number for which display state is to be set or queried. Choose from 1 through 4. |
<char> |
Trace type. Choose from: CLRW - Clear/Write BLANk - Blank MAXH - Max Hold MINH - Min Hold AVG - Average (this parameter only applies to trace averaging.) VIEW - View |
Examples |
TRAC1:TYPE VIEW |
Query Syntax |
:TRACe<n>:TYPE? |
Return Type |
Character |
Default |
CLRW |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
19-sep-2016 |
Added RTSA to relevant modes (A.09.50). |