[:SENSe]:QUANtity:TACTive?

(Read-only) Returns the number of active traces and the number of traces that are currently allowed.

Some SA measurements allow only one measurement trace, such as Channel Mode measurements. In this case, 1,1 would be returned.

Use TRACe<n>:DATA? to read SA trace data.

Use TRACe<n>:TYPE to set the trace type.

Relevant Modes

EMI, SA

Parameters

 

Examples

QUAN:TACT?

'With a general SA measurement active, returns 1,4

'With a Channel power measurement active, returns 1,1

Return Type

Numeric, Numeric

Default

1,4


Last Modified:

20-Oct-2010

New command (5.30)