:TRIGger[:SEQuence]:ATRigger <num>

(Read-Write) Set and query the auto-trigger time. If a trigger signal is not received before the specified auto trigger time, a sweep will occur automatically.

Enable or disable automatic trigger time using :TRIG:ATR:STAT.

Relevant Modes

5GTF, 5G NR, 5G NR EVM Conducted, IQA,LTE FDD, PAA 

Parameters

 

<numeric>

Auto trigger time in seconds.

SA: Choose a value between 0 and 65 seconds.

IQA and RTSA: Choose a value between 1 ms and 100 seconds.

Enter 0 (SA only) to set Auto Trigger OFF. When Auto Trigger is OFF, the FieldFox does NOT sweep unless a valid trigger signal is received.

Examples

TRIG:ATR 2

TRIGger:ATRigger .003

TRIG:ATR 1e2

Query Syntax

TRIG:ATR?

Return Type

Numeric

Default

1.000E+00 (SA)

1.00E-01 (RTSA)

1.000000E-01 (IQA)


Last Modified:

10dec2019

Added 5G NR, 5G NR EVM Conducted, & PAA (11.5x)

28nov2018

Added LTE FDD & 5GTF (11.0)

22-Oct-2017

Added IQA mode (10.1x)

10-june-2016

Added RTSA mode (9.50)

6-Mar-2013

Modified for 6.25