:TRIGger[:SEQuence]:ATRigger:STATe <bool>

(Read-Write) Set and query the auto-triggering state.

Set automatic trigger time using :TRIG:ATR.

Relevant Modes

5GTF, 5G NR, 5G NR EVM Conducted, IQA,LTE FDD, PAA

Parameters

 

<boolean>

Auto trigger state. Choose from:

OFF or 0 - Auto Trigger OFF. The FieldFox does NOT sweep unless a valid trigger signal is received.

ON or 1 - Auto Trigger ON. If a trigger signal is not received before the specified Auto Trig Time (TRIGger[:SEQuence]:EXTernal:ATRigger), a sweep will occur automatically.

Examples

TRIG:ATR:STAT 1

Query Syntax

TRIGger[:SEQuence]:ATRigger:STATe?

Return Type

Boolean

Default

OFF (0)


Last Modified:

10dec2019

Added 5G NR, 5G NR EVM Conducted, & PAA (11.5x)

28nov2018

Added LTE FDD & 5GTF (11.0)

22-Oct-2017

Added IQA mode (10.1x)

10-june-2016

Added RTSA mode (9.50)

6-Mar-2013

Modified for 6.25