TRIGger[:SEQuence]:DELay  <num>

(Read-Write) Set and query the trigger delay time. After a valid trigger signal is received, the sweep begins after the specified Trigger Delay time. Enable Trigger delay using :TRIGger[:SEQuence]:EXTernal:DELay:STATe

Relevant Modes

SA, RTSA

Parameters

 

<num>

Trigger delay time in seconds. Choose a value between 0 and 65 seconds.

Examples

TRIG:DEL 2

Query Syntax

TRIGger[:SEQuence]:DELay?

Return Type

Numeric

Default

0


Last Modified:

10-june-2016

Added RTSA mode (9.50)

6-Mar-2013

Modified for 6.25