:TRIGger[:SEQuence]:EXTernal:DELay:STATe <bool>

(Read-Write) Set and query the trigger delay state. Set delay time using :TRIGger[:SEQuence]:EXTernal:DELay

Relevant Modes

5GTF, 5G NR, 5G NR EVM Conducted, IQA,LTE FDD, PAA

Parameters

 

<bool>

Trigger delay state. Choose from:

OFF or 0 - Trigger delay OFF.

ON or 1 - Auto Trigger ON.

Examples

TRIG:EXT:DEL:STAT 1

Query Syntax

TRIGger[:SEQuence]:EXTErnal:DELay:STATe?

Return Type

Boolean

Default

OFF (0)


Last Modified:

10dec2019

Added 5G NR, 5G NR EVM Conducted, & PAA (11.5x)

28nov2018

Added LTE FDD & 5GTF (11.0)

22-Oct-2017

Added new IQA mode command (10.1x).