:TRIGger[:SEQuence]:EXTernal:DELay <num>

(Read-Write) Set and query the trigger delay time. After a valid trigger signal is received, the sweep begins after the specified Trigger Delay time. Enable Trigger delay using :TRIGger[:SEQuence]:EXTernal:DELay:STATe

Relevant Modes

5GTF, 5G NR, 5G NR EVM Conducted, IQA,LTE FDD, PAA

Parameters

 

<num>

Trigger delay time in seconds. Choose a value between 0 and 65 seconds.

IQA mode:

Minimum: -150 ms

Maximum: 500 ms

Examples

TRIG:EXT:DEL 2

Query Syntax

TRIGger[:SEQuence]:EXTernal:DELay?

Return Type

Numeric

Default

0


Last Modified:

10dec2019

Added 5G NR, 5G NR EVM Conducted, & PAA (11.5x)

28nov2018

Added LTE FDD & 5GTF (11.0)

22-Oct-2017

Added new IQA mode command (10.1x).