:TRIGger[:SEQuence]:EXTernal:SLOPe <char>

(Read-Write) Set and query the trigger slope. Trigger Slope determines which edge of a trigger signal initiates a sweep.

Note: Only valid for VIDeo, EXTernal, and RFBurst triggers.

Relevant Modes

5GTF, 5G NR, 5G NR EVM Conducted, IQA, LTE FDD, PAA

Parameters

 

<character>

Trigger slope. Choose from:

POS  - Sweep is triggered by the rising (positive) edge of signal.

NEG  - Sweep is triggered by the falling (negative) edge of signal.

Examples

TRIG:EXT:SLOP NEG

Query Syntax

TRIGger[:SEQuence]:EXTernal:SLOPe?

Return Type

Character

Default

POS


Last Modified:

10dec2019

Added 5G NR, 5G NR EVM Conducted, & PAA (11.5x)

28nov2018

Added LTE FDD & 5GTF (11.0)

22-Oct-2017

Added new command for IQA mode (10.1x)