Use the Directional-Finding's Map tab to select the define the Acquisition values, Computation Parameters, and Receivers for your measurement.
This topic contains the following sections:
Refer to the following Directional-Finding measurement type(s) for more details:
Measurement Setup (Same as Directional-Finding (Graph and Map) Screen Features)
Acquisition Control (Same as Directional-Finding (Graph and Map) Screen Features)
Measurement Status (Same as Directional-Finding (Graph and Map) Screen Features)
Example of TDoA Measurement Map
Learn more by referring to, Using Time Delay Difference of Arrival (TDoA).