Click View to make the following settings:
Undo/Redo (separate topic)
Toggles the toolbar ON and OFF. When checked, the toolbar is visible. Learn more about these icons.
![]()
Toggles the Status Bar ON and OFF. When checked, the Status Bar is visible in the bottom of the software screen.
![]()
Toggles (ON and OFF) the Trace Data Pane which appears to the left of the chart window.
This ON / OFF setting remains until you change it.
In the Columns Displayed check boxes, select the desired columns to view. The listed data shows the Frequency, e' , e", Loss Tan e, u', u", and Los Tan u for each data point in the active (selected) trace.
When a marker is selected on this trace, its position is coupled with the table data selection.

Limit test compares the measured data with defined limits using the Limit Test Pane, and provides Pass or Fail information for each trace.

The Limit Test Pane allows you to add limit traces and then define limit line points.

Limit Test ON - Switch for turning limit test ON/OFF.
Limit Line ON - Switch for turning limit line display ON/OFF.
Add, Import, Delete - Add, import, or delete a limit line. Import limit lines from a .prn file exported by the N1500A. Its properties can be updated by double clicking in a grid cell.
Add, Delete - Add or delete points of each limit line. Update points by double clicking in a grid cell.
Save, Load, Apply - Save limit test settings to a .xml file and reload them later using the Load button. When the settings have been defined, click Apply to view the results.
(N1500A-004 Only) When clicked, traces appear on the current chart representing the three User-defined standards.