Other Eye Diagram topics
PLTS allows you to specify a synthesized bit pattern (sequence) of between 8 and 32 bits that is convolved with the calculated time domain data to generate the eye diagram.
This dialog appears once for each data set. After that, the same bit pattern is used until you change it.
How to open this dialog again to change the Bit Pattern
Click Tools, then Bit Pattern, then Apply
PRBS Pattern Length Selections |
ABS Pattern Length Selections |
||
|---|---|---|---|
Selection |
Number of Bits |
Selection |
Number of Bits |
2^5-1 |
(31 bits) |
- - |
- - |
2^7-1 |
(127 bits) |
2^7 |
(128 - 2 = 126 bits) |
2^9-1 |
(511 bits) |
2^9 |
(512 - 2 = 510 bits) |
2^10-1 |
(1023 bits) |
2^10 |
(1024 - 2 = 1022 bits) |
2^11-1 |
(2047 bits) |
2^11 |
(2048 - 2 = 2046 bits) |
2^13-1 |
(8191 bits) |
2^13 |
(8192 - 2 = 8190 bits) |
2^15-1 |
(32767 bits) |
2^15 |
(32768 - 2 = 32766 bits) |
2^23-1 |
(8,388,607 bits) |
2^23 |
(8,388,608 - 2 = 8,388,606 bits) |
If the Pattern Length = 2^7 bits, there are 128 unique patterns available if you count in binary from 0 to 127.
0000000
0000001
0000010
.
.
.
1111101
1111110
1111111
PRBS removes 00000000 as invalid.
ABS removes patterns 0000000 and 1111111 as invalid patterns so that you now have a total of 2Pattern Length - 2 = 27 - 2 = 126 unique patterns to choose from. Then ABS uses a random number generator to choose the first pattern to put into the virtual pattern generator and continues to pick new random patterns up to the number of patterns that you have defined within the interface (maximum is 126).
Using both of these values, a random number generator selects unique bit patterns until the appropriate number of patterns are identified. Each of these unique bit patterns are then used to create the eye diagram, one bit pattern at a time.
Beginning with PLTS release 5.0, you can import existing patterns that are saved in the following file types:
DUAL files: *.txt
HEX files: *.txt
Binary files: *.bin
PTRN files: *.ptrn
DAT files: *.dat
PTN files: *.ptn
The maximum file size that can be imported is 64k Bytes..
These patterns can be generated using the FREE Keysight Pattern Editor and Sequencer 3.0 software.
Click Tools, then Bit Pattern, then Import
Import Digital Pattern dialog |
Select File to Import Click Browse, then navigate to the file to be imported. File Description Once selected, the pattern contents appear in the text box, along with Type, format, and number of bits. Import PatternPattern Name Type a pattern name for this file. This name will appear in the 'Choose a Digital Pattern' dialog and also in the title of a displayed eye diagram plot, as in the following image:
Rise/Fall time (pico seconds) Enter the default time that it takes a signal to transition from a low to a high (10% to 90%) condition (or the time that it takes a signal to transition from a high to a low (90% to 10%) condition). This value can be changed each time the bit pattern is used. Data Rate (Gb/S) Enter the default speed in which the pattern is transmitted through your DUT. This value can be changed each time the bit pattern is used. The following image shows examples of how these values are defined:
|
Although several bit patterns are available in PLTS, you can easily create custom bit patterns, from 8 to 32 bits.
How to Design a Custom Bit Pattern
Click Tools, then Bit Pattern, then Design
Digital Pattern Generator dialog |
Click the numerical 'piano' keys to generate a bit pattern up to 32 bits in length. Numeric Representation Choose a numerical format in which to present the data. Save Pattern Enter a filename for the digital pattern. The pattern is saved to folder location specified by the File Storage User Preference. Rise/Fall Time and Data Rate Specify the pulse specifications. The following example shows the specs for a single pulse using 80ps Rise/Fall Time and 2.5 Gb/s Data Rate. Pattern Length (bits) The default value is 32. The allowable range is between 8 and 32 bits. You may change this if your pattern contains fewer bits. If this value is changed to a value less than 32, any remaining bits are ignored. For example if you enter 10 as the pattern length value, then bits 0 through 9 are used and bits 10 through 31 are ignored.
|