Important Notes
|
Click File, then Import, then select either Single File, or Build File (from Multiple Files).
Import a single file into PLTS for data analysis. 1. Select Data Domain to Import: Frequency or Time.
2. Select File Type: Click the down-arrow to import one of the following:
3. Select File to Import: Click Browse to find the file to import. 4. Configuration of Data to Import: Click Change to launch the DUT Configuration dialog.
5. Limit Data Range to Import:
|
Build a single DUT file by importing data from multiple files . The imported data are mapped to various parameters or ports. The subsequent data can then be exported or analyzed by PLTS. 1. Select Data Domain to Import: Frequency or Time. If Time is selected, also type the Stop Frequency to be used in the Fast Fourier Transform algorithm. 20 GHz is the default value, and is best for most applications. 2. Configuration of Data to Import (Build). Click Change to launch the DUT configuration dialog. These changes are reflected in the DUT Configuration diagram in the upper-right corner of the dialog.
3. Select File Type: Click the down-arrow to import one of the following:
4. Select File to Import: Click Browse to find the file to import. 5. Choose Parameter Mapping: In the following field, choose to map either Individual parameters or Ports. Note: To perform NO re-mapping, select Port, then click >> to retain the original port mapping. 6. Select one file parameter to map to one or more selected DUT parameters. This setting allows you to re-map the imported data to alternate DUT ports.
7. Limit Data Range to Import:
Export (Optional) Click to export the remapped data. Click OK to close the dialog. |
Change - Opens the DUT Configuration dialog so you can make changes to your DUT configuration. Browse for Import Build Config File - Opens a file manager window to select a *.csv file of a saved build. Example BuildMultiPortConfig.csv file shown below.
Export - Saves your build as an *.snp file. Note: The folder location can be either an absolute path or a relative path to the folder that contains the configuration file.
|