Write/Read |
About Exporting Data |
Description |
Sets and reads the Start Frequency to use when exporting frequency domain data and ExportDataRange Property is set to Subset. To export data, use ExportFreqDomainTextFileWithSpecifiedDefaults Method. |
VB Syntax |
doc.ExportStartFreqMHz = value |
Variable |
(Type) - Description |
|
doc |
(object) - A PLTSDoc object |
|
value |
(Double) Start frequency (in MHz) of exported data. Must be within the range of the original data. |
Return Type |
Double |
Default |
-1 (Use the start frequency of the original data) |
Examples |
doc.ExportStartFreqMHz = 50 |
C++ Syntax |
HRESULT get_ExportStartFreqMHz(Double *Value); HRESULT put_ExportStartFreqMHz(Double Value); |
Interface |
IPLTSDoc |