Write/Read |
About Exporting Data |
Description |
Sets and reads the Step Time to use when exporting time domain data and ExportDataRange Property is set to Subset. this effectively sets the number of data points exported for each parameter. To export data, use ExportTimeDomainTextFileWithSpecifiedDefaults Method. |
VB Syntax |
doc.ExportStepTimeNs = value |
Variable |
(Type) - Description |
|
doc |
(object) - A PLTSDoc object |
|
value |
(Double) Step time (in Nano seconds) of exported data. |
Return Type |
Double |
Default |
-1 (Use Step time of the original data). |
Examples |
doc.ExportStepTimeNs = 5 |
C++ Syntax |
HRESULT get_ExportStepTimeNs(Double *Value); HRESULT put_ExportStepTimeNs(Double Value); |
Interface |
IPLTSDoc |