Write/Read |
About Exporting Data |
Description |
Sets and reads the Stop Time to use when exporting time domain data and ExportDataRange Property is set to Subset. To export data, use ExportTimeDomainTextFileWithSpecifiedDefaults Method. |
VB Syntax |
doc.ExportStopTimeNs = value |
Variable |
(Type) - Description |
|
doc |
(object) - A PLTSDoc object |
|
value |
(Double) Stop time (in Nano seconds) of exported data. Must be within the range of the original data. |
Return Type |
Double |
Default |
-1 (Use Stop time of the original data). |
Examples |
doc.ExportStopTimeNs = -10 |
C++ Syntax |
HRESULT get_ExportStopTimeNs(Double *Value); HRESULT put_ExportStopTimeNs(Double Value); |
Interface |
IPLTSDoc |