Write-only |
About Bit Patterns |
Description |
Sets a digital pattern for eye diagram generation. |
VB Syntax |
plts.LoadBitPattern Name, dataRate, riseTime, patternLen, amplitude |
Variable |
(Type) - Description |
|
plts |
(object) - A PLTSApplication object |
|
name |
(String) Name of existing bit pattern definition. Choose from: "PRBS" Pseudo-Random Bit Sequence "K 28.5" Industry standard "ABS" Arbitrary Bitstream - a random-like bit stream |
|
dataRate |
(Double) Data Rate (Gb/S) The speed that data is transferred over a circuit or a communications line. |
|
riseTime |
(Double) Rise/Fall Time (pS) The time that it takes a signal to transition from a low to a high (10% to 90%) condition (or the time that it takes a signal to transition from a high to a low (90% to 10%) condition). |
|
patternLen |
(String) Pattern Length (bits) The number of bits in the digital pattern used to create the eye diagram. This value is the limiting factor in creating unique digital patterns. The value of the Pattern Length may be changed for PRBS and ABS. Other defined bit patterns have the Pattern Length defined as part of the pattern and may not be changed except by changing the bit pattern definition.
Learn more. Digital Pattern for Eye Generation dialog. |
|
amplitude |
(Double) Amplitude. The simulated stimulus value in millivolts. |
Return Type |
None |
Default |
None |
Examples |
pltsapp.LoadBitPattern "ABS" |
C++ Syntax |
HRESULT LoadBitPattern(BSTR name, double dataRate, double riseTime, BSTR patternLen, double amplitude); |
Interface |
IPLTSApplication |