Read-Write |
About Eye MaskAbout Limit Lines |
Description |
Loads the specified Limit Line or Eye Mask (*.xml) file. After loading a mask file, wait for the eye diagrams to finish drawing before calling this function. |
VB Syntax |
view.LoadLimitGroup fileName, passFail |
Variable |
(Type) - Description |
|
view |
(object) - A PLTSView object |
|
fileName |
(String) Full path, filename, and suffix (.xml) to load. |
|
passFail |
(Short) [out] Reads the Pass / Fail status. 0 - Fail 1 - Pass |
Return Type |
Short |
Default |
None |
Examples |
view.LoadLimitGroup "C:/PLTS/S11.xml", bPass |
C++ Syntax |
HRESULT LoadLimitGroup(BSTR groupName, SHORT * bPass); |
Interface |
IPLTSView |