The Print feature in the File menu has the following options:
Other Analysis Tools and Utilities Topics
The Print Setup dialog box allows you to set your printer settings to print the displayed PLTS information in the way you choose.
To set the settings for the printer, click File, then Print Setup.
The Print Setup dialog box allows you to change the following basic printer functions:
The printer:Select a new printer from the Name list in the Printer area.
The paper size:Select the paper size from the Size list in the Paper area.
The paper source:Select the paper source from the Source list in the Paper area.
The paper orientation:Select the orientation, either Portrait or Landscape in the Orientation area.

More advanced settings are available by selecting the Properties button or the Network button.
OK -saves the changes that were made, exits the Print Setup dialog box, and returns to the PLTS window.
Cancel - cancels any changes that were made, exits the Print Setup dialog box, and returns to the PLTS window.
The Print Preview option allows you to preview your active plot window before printing the display.
To preview your active plot window before printing, click File, then Print Preview.
The active plot window is displayed for your review.
The second page of the preview screen displays a list of the open DUT files.

In addition to the area to be printed, the screen displays the following seven buttons across the top of the screen.
|
Print: |
Prints the active plot window in the preview screen to the printer. |
|
Next Page: |
Active when One Page is selected. Moves the display to the next page of the display. |
|
Prev Page: |
Active when One Page is selected. Moves the display to the previous page of the display. |
|
One Page or |
Toggles between the two selections. When only one page of the display is shown, Two Page is displayed. When both of the pages of the display are shown, One Page is displayed. |
|
Zoom In: |
Allows you to zoom in on the displayed active plot. |
|
Zoom Out: |
Allows you to zoom out from the displayed active plot. |
|
Close: |
Closes the preview screen without printing. |
The active plot window may be printed to the printer defined in the Print Setup dialog box.
To print the active plot window, click File, then Print.
Make the Print dialog box selections that meet your requirements.
In the Printer area:
Select another printer from the Name list if the displayed printer is not appropriate.
Select the Print to file check box, to save the active plot window as a print (.prn) file rather than printing to a printer.
In the Print range area:
Select All to print all pages.
Select Pages to print specific pages. Then enter the first page to print in the from: entry box and enter the last page to print in the to: entry box.
In the Copies area:
Enter the Number of copies to change the number of copies that you want to print. You may enter a number in the entry box or you may click the spinners (the up arrow and the down arrow at the right edge of the entry box) to change the number of copies.
If the Number of copies entry is greater than "1", you can toggle Collate check box on and off. If the check box has a check, the print copies will be collated.
3. When the Print dialog box entries are correct, click the OK button to print the active plot window.
The Cancel button exits the dialog box without printing and returns to the main PLTS window.
|
Note: The display may also be printed by:
|