Requires Advanced Calibration (5xP) PLTS license.
This feature allows you to load S4P files of Differential Crosstalk TRL Cal and Single-ended TRL standard measurements and then recalculate the Cal Set. The Cal Set is then applied to the current measurement. You might do this to replace the measurement of a standard with one that is more accurate, then recompute the Cal Set.
Here is the process:
Perform or recall a coaxial PNA cal.
Measure the DUT
Call this dialog.
Load the Differential Cross Talk TRL Cal standard measurements. These can be *.S4P files, *.CTI files, or *.DUT files.
Type a name for the new Differential Crosstalk Cal Set (a *.CAL file)
Click Compute Calset and Correction.
The displayed measurement is corrected with the new cal set.
Click Calibration, then Differential Crosstalk Cal, then Calculate Cal Set
|
Calculate Cal Set dialog |
|
Thru Click Reflect. Click Reflect Type: Click the type of reflection standard. LineN Click Start / Stop Freq (MHz) Type the Start and Stop frequencies over which the standard is measured. Symmetric Calkits Check if all of the data files are measured in a symmetric (top/ bottom and left/right) fixture . Different math is used if the fixture is symmetric. Saving Calset to: Click Compute Calset / Correction Click to compute the Calset and apply to the current data file.
|