Where x = F, N, or U. See Software License Types below.
N19301B-1xP/1UL – Base PLTS configuration. Includes the basic User Interface and Analysis-ONLY functionality for up to 4-port data.
N19303B-1xP/1UL – Software control of equipment for calibration and measurement. Requires N19301B.
N19305B-1xP/1UL – Advanced Calibration package: Requires N19301B (for Analysis ONLY) and N19303B (for Instrument control).
N19306B-1xP/1UL - PAM4 analysis. Requires N19301B.
N19307B-1xP/1UL – Greater than 4 ports. The current limit is 32 ports. Requires N19301B (for Analysis ONLY) and N19303B (for Instrument control).
Note: A PLTS Free Trial includes N19301B, N19303B, N19305B, N19306B, and N19307B capability.
Where x = 1, 3, 5, 6, or 7. See Currently Available PLTS Licenses above.
Fixed or Node-Locked (N1930xB-1FP) – This is a license type that is tied to the HOSTID (MAC Address) of the PC that will run the software.
Networkable or Floating (N1930xB-1NP) – This is a license type that is tied to a server. The installation process is pointed to the server and a license is checked out that will run PLTS software.
Transportable or USB Dongle (N1930xB-1UP) – This is a license type that is tied to a USB Dongle or Key that must be present in the PC for the software to run.
N1930A – The original PLTS licenses. They were licensed in two parts. The software license was the N1930A and the SUS was the N1930U.
N1930A-010 – This was the way to order a fully functional (4 port only) node-license with both analysis and measurement.
N1930A-020 – This was the way to order a fully functional (4 port only) floating license with both analysis and measurement.
N1930A-LT1 – Identical to N1930A-010 but without RLGC extraction functionality
N1930A-LT2 – Identical to N1930A-020 but without RLGC extraction functionality
To receive a PLTS software update, you must have an active subscription which is typically renewed annually.
If an SUS is expired, a 2 year SUS must be ordered to reactivate the Subscription.
Previous Support Number |
Description |
New Support Number |
N1930BU-1FP |
12 months of support for PLTS Base Analysis Fixed License |
N19301B+R-A6G-001-L |
N1930BU-1NP |
12 months of support for PLTS Base Analysis Networkable License |
N19301B+R-A6G-002-L |
N1930BU-1TP |
12 months of support for PLTS Base Analysis Transportable License |
N19301B+R-A4G-005-L |
N1930BU-3FP |
12 months of support for PLTS Measurement and Calibration Fixed License |
N19303B+R-A6G-001-L |
N1930BU-3NP |
12 months of support for PLTS Measurement and Calibration Networkable License |
N19303B+R-A6G-002-L |
N1930BU-3TP |
12 months of support for PLTS Measurement and Calibration Transportable License |
N19303B+R-A6G-005-L |
N1930BU-5FP |
12 months of support for PLTS Advanced Calibration Fixed License |
N19305B+R-A6G-001-L |
N1930BU-5NP |
12 months of support for PLTS Advanced Calibration Networkable License |
N19305B+R-A6G-002-L |
N1930BU-5TP |
12 months of support for PLTS Advanced Calibration Transportable License |
N19305B+R-A6G-005-L |
N1930BU-6FP |
12 months of support for PAM-4 analysis fixed license |
N19306B+R-A6G-001-L |
N1930BU-6NP |
12 months of support for PAM-4 analysis networkable license |
N19306B+R-A6G-002-L |
N1930BU-6TP |
12 months of support for PAM-4 analysis transportable license |
N19306B+R-A6G-005-L |
N1930BU-7FP |
12 months of support for PLTS N-Port Measurement and Analysis Fixed License |
N19307B+R-A6G-001-L |
N1930BU-7NP |
12 months of support for PLTS N-Port Measurement and Analysis Networkable License |
N19307B+R-A6G-002-L |
N1930BU-7TP |
12 months of support for PLTS N-Port Measurement and Analysis Transportable License |
N19307B+R-A6G-005-L |
Important Note: Please keep your entitlement certificates in a safe place. The order number on the original entitlement certificate is the key to managing and receiving licensing support.