This VBScript example creates IMD power and IM3 measurements, sets sweep mode to Center Frequency Sweep, and performs an IMD cal.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save it on the PNA hard drive as IMD.vbs.
You can see the VB Script program on the PNA that produces an IM spectrum channel from the Marker function at : C:/“/Program Files/Keysight/Network Analyzer/Applications/IMD/IMD.VBS”.
Learn how to setup and run the macro.
|
option explicit 'declare variables dim SweepMode, StartDeltaFreq, StopDeltaFreq, NumFreqs, TonePower, CWFreq dim app, hostname '' Sweep type: '' naIMDToneCWSweep = 0 '' naIMDTonePowerSweep = 1 '' naIMDToneCenterFreqSweep = 2 '' naIMDDeltaFrequencySweep = 3 '' naIMDToneSegmentSweep = 4 'init variables SweepMode = 3 ' Sweep DeltaF StartDeltaFreq = 100e3 StopDeltaFreq = 1e9 NumFreqs = 201 TonePower = -7 CWFreq = 5e9 ' get host name from commandline dim objargs set objargs = wscript.arguments if(objargs.Count = 1) then hostname = objargs(0) set app = CreateObject("Agilentpna835x.application", hostname) call SetupIMD call CalIMD '''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''' '' Create and Configure IMD channel '''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''''' sub SetupIMD dim chan, imd app.reset ' Create IMD measurements app.CreateCustomMeasurementEx 1, "Swept IMD", "PwrMain", 1 app.CreateCustomMeasurementEx 1, "Swept IMD", "IM3", 1 set chan = app.channels(1) chan.hold 1
set imd = chan.CustomChannelConfiguration imd.SweepType = SweepMode imd.FrequencyCenter = CWFreq imd.DeltaFrequencyStart = StartDeltaFreq imd.DeltaFrequencyStop = StopDeltaFreq imd.TonePower(0) = TonePower 'F1 power imd.TonePower(1) = TonePower 'F2 power
chan.NumberOfPoints = NumFreqs chan.single 1 end sub sub CalIMD dim chan, CalMgr, IMDCal, IMDCustomCal, CalSteps, I, CalSet set chan = app.ActiveChannel set CalMgr = app.GetCalManager set IMDCal = CalMgr.CreateCustomCalEx(1)
'Configure IMD GuidedCal for the connector types and ECal module that will be used ' Substitute appropriate connector type and ECal identification strings here IMDCal.Initialize 1, true 'channel number is 1 IMDCal.ConnectorType(1) = "APC 3.5 female" IMDCal.ConnectorType(2) = "APC 3.5 male" IMDCal.CalKitType(1) = "N4693-60001 User 2 ECal 00012" IMDCal.CalKitType(2) = "N4693-60001 User 2 ECal 00012"
' IMD Custom settings set IMDCustomCal = IMDCal.CustomCalConfiguration
' Set the Power Level at the power sensor to be used in calibration IMDCustomCal.PowerLevel = 0
' Specify the connector type of the power sensor. If there is an adapter between ' the input port and the power sensor, specify the connector type here, and set ' the appropriate cal kit type for the connector so that extra calibration can be ' performed. To skip the calibration for the adapter, set PowerSensorConnectorType to "Ignored" ' i.e.: IMDCustomCal.PowerSensorConnectorType = "Ignored" IMDCustomCal.PowerSensorConnectorTYpe = "APC 3.5 female" IMDCustomCal.PowerSensorCalKitType = "N4693-60001 User 2 ECal 00012"
' Set the Max product to calibrate, valid values are 3, 5, 7, and 9 IMDCustomCal.MaxProduct = 3
' Set the calibration Frequencies, can choose between calibrate only at center Frequencies (0) ' or calibrate at all frequencies (1). IMDCustomCal.CalibrationFrequencies = 1
'Include 2nd order product in calibration IMDCustomCal.Include2ndOrderProduct = true
CalSteps = IMDCal.GenerateSteps for I = 1 to CalSteps msgBox IMDCal.GetStepDescription(I) IMDCal.AcquireStep(I) next CalSet = IMDCal.GenerateErrorTerms msgBox "IMD Cal Done" end sub |
Last Modified:
|
31-Mar-2009 |
MX New topic |