Controls the Swept IMD Application settings.
See Properties to set for each sweep type.
|
Dim app as AgilentPNA835x.Application Set app = CreateObject("AgilentPNA835x.Application") app.CreateCustomMeasurementEx(1, "SweptIMD", "PwrMain", 1) Dim IMD Set IMD = app.ActiveChannel.CustomChannelConfiguration |
Example Program Create and Cal a Swept IMD Measurement
Use std channel commands to set source and receiver attenuation.
Method |
InterfaceSee History |
Description |
|---|---|---|
|
ISweptIMD |
Sets port mapping |
|
Property |
Interface |
Description |
|
ISweptIMD |
Sets and returns the method by which CTB and CSO calculations are performed. |
|
|
ISweptIMD |
Sets and returns the CSO Power. |
|
|
ISweptIMD |
Sets and returns the CTB Power. |
|
|
ISweptIMD |
ON | OFF state of power coupling for F1 and F2. |
|
|
ISweptIMD |
Sets the “N = number of distortion products” value for the calculation of the CSO parameter. |
|
|
ISweptIMD |
Sets and returns the offset that is applied to CSO measurements. |
|
|
ISweptIMD |
Sets and returns the offset that is applied to CTB measurements. |
|
|
ISweptIMD |
Sets the “N = Total number of carriers” value used in the calculation of the XMOD and CTB parameter. |
|
|
ISweptIMD |
Fixed tone spacing value. |
|
|
ISweptIMD |
Start spacing of the main tones. |
|
|
ISweptIMD |
Stop spacing of the main tones. |
|
|
ISweptIMD |
Reads input port map |
|
|
ISweptIMD |
Reads output port map |
|
|
ISweptIMD2 |
Superseded with LevelingMethod Set Equal Tone Power state. |
|
|
ISweptIMD |
Frequency of the F1 tone. |
|
|
ISweptIMD |
Frequency of the F1 tone. |
|
|
ISweptIMD |
Center frequency of the main tones. |
|
|
ISweptIMD |
Sweep center frequency when sweeping the main tones. |
|
|
ISweptIMD |
Frequency span when sweeping the main tones. |
|
|
ISweptIMD |
Start frequency when sweeping the main tones. |
|
|
ISweptIMD |
Stop frequency when sweeping the main tones. |
|
|
ISweptIMD4 |
Reads the state of whether or not 2nd order parameters are measured. |
|
|
ISweptIMD |
Reads the highest product that can be measured by SweptIMD. |
|
|
ISweptIMD4 |
Reads the highest product measured by SweptIMD. |
|
|
ISweptIMD |
IF Bandwidth for measurement of the intermodulation products. |
|
|
ISweptIMD3 |
Set power leveling mode |
|
|
ISweptIMD |
IF Bandwidth for measurement of the Main tones. |
|
|
ISweptIMD |
Type of sweep for a Swept IMD measurement. |
|
|
ISweptIMD |
Power level of the Main Tones. |
|
|
ISweptIMD2 |
Superseded with LevelingMethod Set power level at DUT Input or Output |
|
|
ISweptIMD |
Start power level of the Main tones. |
|
|
ISweptIMD |
Stop power level of the Main tones. |
RoleDevice Property to use an external source for f2.
The following commands are relevant for each IMD sweep type:
0 - naIMDToneCWSweep
1 - naIMDTonePowerSweep
2 - naIMDToneCenterFreqSweep
3 - naIMDDeltaFrequencySweep
4 - naIMDToneSegmentSweep (Not available for IMDx)
Also use standard segment sweep commands
5 - naLOPowerSweep (IMDx ONLY)
converter.LOStartPower Property
converter.LOStopPower Property
|
Interface |
Introduced with PNA Rev: |
|
ISweptIMD |
8.33 |
|
ISweptIMD2 |
9.40 |
|
ISweptIMD3 |
9.80 |
|
ISweptIMD4 |
10.60 |